내용 건너뛰기

제품 선택 도우미
제품번호: 0202889 5 제품

Feed adapter D=32, piFLOW® i/f

It is important to optimize the feeding point (where the product is conveyed from) for the conveying system to assure maximum capacity and safe transport. The feed adapter is used to add the optimum amount of air to the material flow. It is adjusted to the bottom of a bag dump station (when it is in use), or other equipment such as sieves, big bag stations, mixers, or containers. It features an adjustable air inlet that helps to control the phase of the conveying. If faster conveying is required and the material is not sensitive, dilute phase is needed. In the case of a delicate product, dense phase conveying has to be reached. The air inlet may be covered with Piab Air inlet filters when the risk of cross-contamination needs to be eliminated.

더 읽기

제품

Show all (5)

특장점

0

모두 제거

Choose your language

비교 제품이 아닙니다

다른 제품 타입은 비교할 수 없습니다. 선택하신 제품들을 제거하시겠습니까?

건의사항
This site is protected by reCAPTCHA and the Google Privacy Policy and Terms of Service apply.